Hi champs,
customer found some abnormality by measuring internal volatge in series production by ADC of TMS320F28335ZJZQ.
So they tested boards with a defined input volatge 1.5V:
First lot of pcbs deviation was ~-0.18%
2nd lot deviation deviation was +0.05%.
They used ASDC_cal() and am additonal external 2.048 reference voltage,
As they said, they used all tipps and workarounds, we provided.
Q1: Can you check, if these measured values are in expected tolerance window ?
|
Microcontroller |
ADCREFSEL |
ADCOFFTRIM |
deviation @ 1.5V |
|
TMS320F28335ZJZQ CA-63ZRH93 |
0x62A1 |
0x01FE |
-0.18% |
|
TMS320F28335ZJZQ CA-5CZDJ43 |
0x5B21 |
0x1FF |
+0.95% |
Q2: is very MCU'S ADC on wafer calibrated ? How is it done, which deviation can be expected ?
3/5/18[LE]>unlock