Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Hello everyone,
I am trying to convert signals for my future application. For the moment I can acquire 4 measures (SOC0 - SOC3) from ADCa, I am using PWM1 (20Khz) SOCA for triggering ADCa and my problem is that the ADC take 33us for make 4 measures ... it's about 121 kSps lots of under the device max.
My configuration is there :
SYSCLK = 200 MHz
ADCCLK = 200/5 = 40 MHz
12 bits mode
ACQPS = 65 (the same for all SOC, so I think I am in synchronous mode)
Interrupt on SOC3 EOC for saving result in a buffer
Run from flash in standalone mode
GPIO31 (led on experimenter card) is used with an oscilloscope (toggle time measuring)
Have you got advice for increasing acquisition speed please ? I need to have four SOC results in less than 5us (if possible). Do you think it is an ADC problem, a memory access speed or a GPIO toggling speed ?
Thank you very much
Best regards,
Jérémy