Hello C2000 team,
I have a customer who would like to configure the HRPWM as follows:
PWMxA - high res frequency control
PWMxB - complement of PWMxA with deadband
PWM signals are active high
It is critical that the frequency resolution of both output signals is not compromised. The size of the deadband between the two output signals should not be a major concern, they just need to be guaranteed to not overlap.
I see there are two places where I could configure this inversion, with the HRCNFG register (SELOUTB), and also in DBCTL register POLSEL field. What is the proper way to configure this inversion and the deadband generator to maximize the frequency resolution?
Thanks,
Munan