This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: TIDM1000 PWM

Part Number: TMS320F28379D

Hi, below is the PWM structure of TIDM1000. I wonder if I can combine phase 2 and 4 together by turning on and off both mosfets at the same time. It will result in higher efficiency since Rdson is smaller in MOSFET than the diode, and we can use only 3 PWM pins of C2000 instead of 3 pairs.

  • Howard,

    Yes, that is a possibility, we wanted the user to have the flexibility in case they are using a device with different characteristics where switching losses might be higher or reverse current flow cannot occur. Hence the design routes both the signals separately. However, in the switching scheme, they are driven together

    regards
    Manish