Part Number: TMS320F28377S
Tool/software: Code Composer Studio
Hello,
I have used the LAUNCHXL LaunchPad-F28377S adapting the multi day workshop developed to the F28379D for learning and knowledge. I was successful until the Lab 9, which uses the CLA, but only managed to make it work when I changed the code that was in interruption CLA1_1_ISR for interruption CLA1_5_ISR in the DefaultIsr_9_10.c file.
I would like some help or hint of what could be the problem because everything else seems to work properly.
Why the interrupption would be happening at the CLA1_5_ISR and not at the CLA1_1_ISR as programed?
If it is necessary, I can provide some more detailed information.
Thanky in advance,
Pedro A.