This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: Cannot Connect with Controller

Part Number: TMS320F28335

Tool/software: Code Composer Studio

I use the TMS320F28335 Experimenters-Kit. I bought a new Control Card (with F28335) for it but I cannot establish a connection using CCS V7.0. I always get the error: "Error connecting to the target: (Error -1135 @ 0x0). The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.48.0)". My other control card works without any problems. The switches on the control cards are in the same position.