This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28374S: Boot ROM status code

Part Number: TMS320F28374S

Hi,

Regarding Boot ROM status code (saved in RAM at address 0x0000002c, documented in Technical Reference Manual section 3.9.9.1):

My application checks this value on start-up to determine whether POR bit in RESC register was cleared by the boot ROM. This helps determine reset type (power-on or via External Reset line), and works as expected.

Question: is this RAM location and bit assignments guaranteed not to change if TI revises the boot ROM code?

Thank you!

-Pavel