Part Number: INSTASPIN-BLDC
Other Parts Discussed in Thread: CONTROLSUITE, DRV8301, DRV8323, MOTORWARE,
Hello,
I am using F28069M and drv8301/drv8323 kit. Recently I was evaluating instaSPIN-FOC, but now i need to compare the performance of FOC and simple trapezoidal commutation. For this purpose I want to load instaSPIN -BLDC project and GUI. In the forum I have found that this can be done by loading examples from ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128. However only the project "PM-sensorless" contains the F2806x RAM configuration options and included files. But this project uses FOC, so for simple trapezoidal control I want to use BLDC project, which has F2803x Option only..
What steps should I do in order to run BLDC on F28069M launchpad?
And how about IQmath which was built in F28xxx (without F/M) devices and isn't in F or M devices like in F28069M. How should I migrate to F or M device at this point?