Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello there,
I own a LaunchPad-XL TMS320F28379D and I have imported "eqep_pos_speed_cpu01" example from C2000Ware. I have no problems building and running the project. Absolutely no changes have been made to the code. I am using graph to read the values of theta_raw which is practically the value of QPOSCNT register. However I don't notice a reset when the index pulse comes out of the GPIO4. I have tested the connections with an oscilloscope an everything seems right. I am attaching a screenshot of the graph. Shouldn't theta_raw reset to 0 when the index pulse comes out? Should I change the value of an eqep register to force reset on index? Thanks for your time.