Other Parts Discussed in Thread: BOOSTXL-DRV8301, DRV8301, MOTORWARE,
Dear all
I'm sorry for repeating the old question regarding jumpers setting in Piccolo. But in spite of reading many papers and watching training movies from Ti pages, jumper settings in Piccolo C2000 is still unclear for me!
My first experiments concerned simple examples related to 28027F launchpad board only.
The supply came from usb thus I have to keeep jumpers 1,2,3 connected as well as switches 1,2,3 = On; ON; ON the same with fat SW4 = ON.
Everything went good, I was able to program and play with the board.
Next stage of my project was to go to the full package - launchpad connected with the boostpack BOOSTXL-DRV8301 and the motor
I tried to go through the example "Getting Started - InstaSPIN-FOC enabled C2000 LP - Motor BP" from https://training.ti.com/getting-started-instaspin-foc-enabled-c2000-lp-motor-bp
According to this example JP1 nad JP2 should be removed, (no sure... JP3 too?) all SW 1,2,3 ON ... and also SW4 ON:
But his configuration fails, when I try to use the InstaSpin GUI...
on the other hand... in "BOOSTXL-DRV8301 Hardware User's Guide " we have:
the same in: "Motor Drive BoosterPack Quick Start Guide: BOOSTXL-DRV8301 "
But, I'm afraid, in this case, SW4 OFF will block the programming/ debuging of the board.
I'm afraid SW4 position is my problem... I know, it's easy to check the right position changing the configuration, but I'm afraid that experiments with jumpers rise the risk of burning launchpoad or USB port in the PC...
Regards,
Marek