Part Number: TMS320F28335
Other Parts Discussed in Thread: CONTROLSUITE,
Tool/software: Code Composer Studio
I am working with below code (from fixed point library of control suite). The code is not working to do real time FFT. please help me to get FFT components for signal given on ADC A0.
// ========================================================================
// This software is licensed for use with Texas Instruments C28x
// family DSCs. This license was provided to you prior to installing
// the software. You may review this license by consulting a copy of
// the agreement in the doc directory of this library.
// ------------------------------------------------------------------------
// Copyright (C) 2010-2011 Texas Instruments, Incorporated.
// All Rights Reserved.
// ========================================================================
//
// File: Main.c -- Real-time RFFT with 12-bit ADC Input Test Example
//
// TITLE: DSP2833x Device Real-time Real FFT Test Program.
//
//=========================================================================
// DESCRIPTION:
//
// This program shows how to compute a real FFT with 12-bit real-time ADC
// input and associated spectrum magnitude, phase. The input data is
// collected by interrupt service routine function adc_isr(). The signal
// input (can be any signal from signal generator or sensor) is excerted
// in ADC input A0. The signal is sampled by epwm module and sampling
// frequency is defined in Lab.h. Here is 48kHz. The dynamic range of the
// input signal should be less than 0~3V. Real time real FFT is conducted
// frame by frame. As long as one frame of data is collected by adc_isr,
// it will set the FFTStartFlag. Whenever the main program detect the
// FFTStartFlag set, the FFT calculate starts. The FFTStartFlag is cleared
// after the calculation finished.
//
// The input buffer must be aligned to a multiple of the FFT size if using
// RFFT_adc_f32. If you do not wish to align the input buffer then use the
// RFFT_adc_f32u function. In this case, the section alignment #pragma can
// be commented. However, using this function will reduce cycle performance
// of the algorithm.
//
//
// FUNCTIONS:
//
// void RFFT_adc_f32 (RFFT_ADC_F32_STRUCT *)
// void RFFT_f32_mag (RFFT_F32_STRUCT *)
// void RFFT_f32_phase (RFFT_F32_STRUCT *)
//
// Where RFFT_ADC_F32_STRUCT is a structure defined as:
//
// typedef struct {
// Uint16 *InBuf;
// void *Tail;
// } RFFT_ADC_F32_STRUCT;
//
// Where RFFT_F32_STRUCT is a structure defined as:
//
// typedef struct {
// float32 *InBuf;
// float32 *OutBuf;
// float32 *CosSinBuf;
// float32 *MagBuf;
// float32 *PhaseBuf;
// Uint16 FFTSize;
// Uint16 FFTStages;
// } RFFT_F32_STRUCT;
//
// ASSUMPTIONS:
//
// * OutBuf of RFFT_F32_STRUCT has to be passed to Tail of
// RFFT_ADC_F32_STRUCT
// * Input signal is stored in Signal.asm
// * FFTSize must be a power of 2 (32, 64, 128, etc)
// * FFTSize must be greater or equal to 32
// * FFTStages must be log2(FFTSize)
// * InBuf, OutBuf, CosSinBuf are FFTSize in length
// * MagBuf and PhaseBuf are FFTSize/2+1 in length
// * MagBuf and PhaseBuf are not used by this function.
// They are only used by the magitude and phase calculation functions.
//
// Watch Variables:
//
// InBuf(RFFT_ADC_F32_STRUCT) Input buffer
// InBuf(RFFT_F32_STRUCT) Not used
// Tail Stored the address of OutBuf
// OutBuf Output buffer
// CosSinBuf Twiddle factor buffer
// MagBuf Magnitude buffer
// PhaseBuf Phase buffer
// j Index of normalized digital frequency component
// freq Real analog frequency of raw signal
//
//###########################################################################
// $TI Release: C28x Floating Point Unit Library V1.30 $
// $Release Date: January 04, 2012 $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#include "math.h"
#include "float.h"
#include "FPU.h"
#define RFFT_STAGES 9
#define RFFT_SIZE (1 << RFFT_STAGES)
#define ADC_BUF_LEN RFFT_SIZE // ADC buffer length
#define ADC_SAMPLE_PERIOD 3124 // 3124 = (3125-1) = 48 KHz sampling w/ 150 MHz SYSCLKOUT
#define F_PER_SAMPLE 48000.0L/(float)RFFT_SIZE //Internal sampling rate is 48kHz
RFFT_ADC_F32_STRUCT rfft_adc;
RFFT_F32_STRUCT rfft;
float32 RFFToutBuff[RFFT_SIZE]; //Calculated FFT result
float32 RFFTF32Coef[RFFT_SIZE]; //Coefficient table buffer
float32 RFFTmagBuff[RFFT_SIZE/2+1]; //Magnitude of frequency spectrum
//--- Global Variables
Uint16 AdcBuf[ADC_BUF_LEN]; // ADC buffer allocation
volatile Uint16 FFTStartFlag = 0; // One frame data ready flag
Uint16 DEBUG_TOGGLE = 1; // Used in realtime mode investigation
// Prototype statements for functions found within this file.
interrupt void adc_isr(void);
/**********************************************************************
* Function: main()
*
* Description: Main function for C2833x Real-time RFFT
**********************************************************************/
void main(void)
{
Uint16 i,j;
float32 freq; // Frequency of single-frequency-component signal
//--- CPU Initialization
InitSysCtrl(); // Initialize the CPU (FILE: SysCtrl.c)
InitGpio(); // Initialize the shared GPIO pins (FILE: Gpio.c)
InitPieCtrl(); // Initialize and enable the PIE (FILE: PieCtrl.c)
//--- Peripheral Initialization
InitAdc(); // Initialize the ADC (FILE: Adc.c)
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
rfft_adc.Tail = &rfft.OutBuf; //Link the RFFT_ADC_F32_STRUCT to
//RFFT_F32_STRUCT. Tail pointer of
//RFFT_ADC_F32_STRUCT is passed to
//the OutBuf pointer of RFFT_F32_STRUCT
rfft.FFTSize = RFFT_SIZE; //Real FFT size
rfft.FFTStages = RFFT_STAGES; //Real FFT stages
rfft_adc.InBuf = &AdcBuf[0]; //Input buffer
rfft.OutBuf = &RFFToutBuff[0]; //Output buffer
rfft.CosSinBuf = &RFFTF32Coef[0]; //Twiddle factor
rfft.MagBuf = &RFFTmagBuff[0]; //Magnitude output buffer
RFFT_f32_sincostable(&rfft); //Calculate twiddle factor
//Clean up output buffer
for (i=0; i < RFFT_SIZE; i++)
{
RFFToutBuff[i] = 0;
}
//Clean up magnitude buffer
for (i=0; i < RFFT_SIZE/2; i++)
{
RFFTmagBuff[i] = 0;
}
//--- Enable global interrupts
asm(" CLRC INTM, DBGM"); // Enable global interrupts and realtime debug
//--- Main Loop
while(1) // endless loop - wait for an interrupt
{
if(FFTStartFlag) // If one frame data ready, then do FFT
{
RFFT_adc_f32u(&rfft_adc); // This version of FFT doesn't need buffer alignment
RFFT_f32_mag(&rfft); // Calculate spectrum amplitude
j = 1;
freq = RFFTmagBuff[1];
for(i=2;i<RFFT_SIZE/2+1;i++)
{
//Looking for the maximum valude of spectrum magnitude
if(RFFTmagBuff[i] > freq)
{
j = i;
freq = RFFTmagBuff[i];
}
}
freq = F_PER_SAMPLE * (float)j; //Convert normalized digital frequency to analog frequency
FFTStartFlag = 0; //Start collecting the next frame of data
}
asm(" NOP");
}
} //end of main()
interrupt void adc_isr(void)
{
static Uint16 *AdcBufPtr = AdcBuf; // Pointer to ADC data buffer
static volatile Uint16 GPIO34_count = 0; // Counter for pin toggle
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Must acknowledge the PIE group
//--- Manage the ADC registers
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1 to CONV00 state
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear ADC SEQ1 interrupt flag
//--- Read the ADC result
*AdcBufPtr++ = AdcMirror.ADCRESULT0; // Read the result
//--- Brute-force the circular buffer
if( AdcBufPtr == (AdcBuf + ADC_BUF_LEN) )
{
AdcBufPtr = AdcBuf; // Rewind the pointer to the beginning
FFTStartFlag = 1; // One frame data ready
}
//--- Example: Toggle GPIO18 so we can read it with the ADC
if(DEBUG_TOGGLE == 1)
{
GpioDataRegs.GPATOGGLE.bit.GPIO18 = 1; // Toggle the pin
}
//--- Example: Toggle GPIO34 at a 0.5 sec rate (connected to the LED on the ControlCARD).
// (1/48000 sec/sample)*(1 samples/int)*(x interrupts/toggle) = (0.5 sec/toggle)
// ==> x = 24000
if(GPIO34_count++ > 24000) // Toggle slowly to see the LED blink
{
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1; // Toggle the pin
GPIO34_count = 0; // Reset the counter
}
return;
} //end of main()
//===========================================================================
// End of File
//===========================================================================