Hello,
I have a question about power sequence of TMS320F280049.
The datasheet specify the power sequence as below.
"When using an external source to supply VDD, the voltage on VDDIO must be greater than VDD or no less than 0.3 V below VDD at all times."
On the customer's system, the power up sequence is keep the datasheet requirement, but power down sequence cannot meet it.
VDDIO 3.3V become to lower voltage than VDD 1.2V in the process of power down sequence due to the errata about the VDD supply as below.
"VDD Supply: During VDDIO Power Up, VDD May Also Rise"
-During the power down sequence, VDDIO < VDD. Is it problem? Due to the errata, it is difficult to keep the condition of VDDIO > VDD during the power down sequence.
-Any plan to fix this errata?
Regards,
Furuya