Other Parts Discussed in Thread: C2000WARE
Sir,
This is Regarding the given Example code for the processor, I tried to use the eQEP module for speed measurement for 3Phase ACI motor(around 5KW).
The issue is this when I measure the speed with externally powered the motor, the speed measurement is very good. But when I started my Inverter with DC link of around 500 volts, the speed measurement goes wrong even very wrong.
I tried to find out the issue and I found that when the inverter starts the qep signal picking high-frequency noise and this not is very easily picked up by the processor's eqep module and make the speed measurement wrong.
So Is there is any solution which eliminates the noise. I want to measure Eqep real pulse only.
Ashutosh