Part Number: TMS320F28379D
Hi,
Question regarding GPIO pins assignment in Position Manager (PM) library for serial encoder i.e. EnDat 2.2, BiSS-C and T-Format.
EnDat 2.2: sprui35.pdf -> See Figure 2 on Page 6 and Table 6 on Page 33
BiSS-C: sprui37.pdf -> See Figure 3 on Page 6 and Table 9 Page 18
T-Format: sprui71.pdf -> See Figure 2 on Page 6 and Table 6 on Page 20
1. Can I use any other GPIO, other than GPIO 6 and 7 for ENDAT_CLK and SPICLK?
2. Is EPWM4 fix for encoder PM Lib and can output of the EPWM4 can be configure to other GPIO for position manager?
3. Also instead of GPIO 34, can any other GPIO be assigned and map to OUTPUTXBAR1?
4. Does SinCos PM Lib (see sprui54.pdf) uses CLB?
Thanks
PJ