Hi Champs,
During my recent customer visit, several digital power customers are developing higher performance products, whose PWM frequency would be higher than 500KHz(100KHz ISR frequency at least), and maybe 1MHz when using GaN devices. The topology is LLC or PSFB. So they are asking whether current 200MHz C2000 device can deal with this challenge? If not, how to design the architecture using C28x and CLA, maybe CLA and C28x process parallel. Do we have example code or plan to develop?
On the other side, I asked customer to test the execution time of their PWM ISR using the latest C2000 device.
Thanks.
BR,
Young