This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28377S: Target Hardware in Simulink, cannot select Group SPI_A

Part Number: LAUNCHXL-F28377S

Hello,

I am using the TI Delfino F28377S in Simulink and CAN, ADC and so on is working very well.

Today I tried to get SPI running, but first I had to select the SPI Block from another Support Package (TI 280x) and when I tried to compile, there was this mistake:

Error evaluating 'InitFcn' callback of C28x SPI Receive block (mask) 'LauchPadXL_xxx/SPI Receive'.
Caused by:
Reference to non-existent field 'SPI_A'.

So this comes from inserting a block from another controller and because the SPI_A interface is not listed in the configurations of the Hardware...

Can someone please help? I ordered the board, because it promised to be able to use SPI via Simulink.

Greetings from Germany