Other Parts Discussed in Thread: DRV8301-69M-KIT, , INSTASPIN-BLDC, BOOSTXL-DRV8305EVM, LAUNCHXL-F28069M, TMDSCNCD28035ISO, MOTORWARE
Hey guys!
I am trying to understand the datasheet information of some of the motor control development kits so I can pick the right board/s.
here are the three boards I have been looking into:
DRV8301-69M-KIT -- 18V to 60V, 40A
TMDSHVMTRINSPIN -- 50V to 350V, 10A (This board has been rated 1.5kW)
DRV8301-HC-C2-KIT -- 18V to 60V, 60A
Here are my questions:
1- How these voltage and currents relate to the output power of the kits? (e.g. in case of TMDSHVMTRINSPIN P=10x50=500W or P=350x10=3.5kW or the P=1.5kW and I can set the rated voltage between 50-350 and the current will be calculated accordingly, OR??!!)
2- Can I get a InstaSpin BLDC for either DRV8301-HC-C2-KIT or DRV8301-69M-KIT? What would be the DIMM100 control board?
Thanks
What is the output power when the voltage range is 18-350V and max current is claimed to be 10A continuous?