Part Number: TMS320F28377S
I am not seeing an GPIO intput pin change state in the microcontroller even though I can probe it and confirm the state change on the board. This problem only happens when I setup the pin to have an input pull up. I have a 10K pull up on my circuit externally. When i set the PUD to disable pull up internally I can detect the state change. Why is this the case?
Thanks,
Rohit.