Part Number: TMS320F28377D
We have been working on TI's FPU library "c28x_fpu_dsp_library" V1.5 on TMS320F28377 dsp.
Below attached is a picture of library's user guide related to "CFFT_f32" function.
What does the highlighted note means?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377D
We have been working on TI's FPU library "c28x_fpu_dsp_library" V1.5 on TMS320F28377 dsp.
Below attached is a picture of library's user guide related to "CFFT_f32" function.
What does the highlighted note means?
Only if they call the CFFT_f32 function or modify any of the global variables it uses. Otherwise there should be no problem.
Regards,
Richard
What do you mean by global variables?
As per my knowledge this are the variables are as below.
typedef struct
{
float32 *InPtr; //!< Pointer to the input buffer
float32 *OutPtr; //!< Pointer to the output buffer
float32 *CoefPtr; //!< Pointer to the twiddle factors
float32 *CurrentInPtr; //!< Points to input buffer at each FFT stage
float32 *CurrentOutPtr; //!< Points to output buffer at each FFT stage
uint16_t Stages; //!< Number of FFT stages
uint16_t FFTSize; //!< Size of the FFT (number of complex data points)
} CFFT_F32_STRUCT;
float32 CFFTin1Buff[CFFT_SIZE * 2];
float32 CFFToutBuff[CFFT_SIZE * 2];
float32 CFFTmagBuff[CFFT_SIZE];
float32 CFFTF32Coef[CFFT_SIZE];
CFFT_F32_STRUCT cfft;
CFFT_F32_STRUCT_Handle hnd_cfft;
Are there any other global variables used by CFFT_f32 function?
We are facing a problem. You can refer this thread for reference
Actually CFFT_f32() function is not called based on interrupt, rather its calling is done in background at every 20mSec.
CFFT_f32() function execution time :
180 uSec with all interrupt disabled.
324 uSec with only timer0 disabled(interrupt group1 enabled).
We performed three different test logic as below:
Test 1:
We kept timer0 interrupt enabled with no code written in ISR as shown below:
GpioDataRegs.GPESET.bit.GPIO133 = 1; CpuTimer0Regs.TCR.bit.TIF = 1; PieCtrlRegs.PIEACK.bit.ACK1 = 1; //Timer0_ISR_rout(); GpioDataRegs.GPECLEAR.bit.GPIO133 = 1;
But problem still occurred.
Test 2:
We tested it with keeping interrupt group1 enabled but disabling timer0 interrupt before calling of CFFT_f32() function as shown below.
CpuTimer0Regs.TCR.bit.TIE = 0; //Timer interrupt disable. GpioDataRegs.GPBSET.bit.GPIO45 = 1; hnd_cfft->InPtr = CFFTin1Buff; hnd_cfft->OutPtr = CFFToutBuff; CFFT_f32(hnd_cfft); GpioDataRegs.GPBCLEAR.bit.GPIO45 = 1; CpuTimer0Regs.TCR.bit.TIE = 1;
After this we did not observe problem occurrence.
Test 3:
Then we disabled timer0 interrupt and it's clock, and use EPWM10_INT_ISR(group 3) for our purpose of 200 uSec interrupt as below:
Uint16 Prev_IER = IER; GpioDataRegs.GPETOGGLE.bit.GPIO133 = 1; //Timer0_ISR_rout(); EPwm10Regs.ETCLR.bit.INT = 1; PieCtrlRegs.PIEACK.bit.ACK3 = 1; Prev_IER |= IER_GROUP3; IER = Prev_IER;
But problem still occurred.
This problem has consumed lots of time and its urgent, so kindly provide guidance as soon as possible.
Thank for your response.
You can refer attached code of CPU-1 and CPU-2. In which we are facing problem in output of CFFT_f32 function.
In periodically call of CFFT_f32 function, most time it gives correct magnitude of given 5th and 7th harmonics order.
but at some random instance it is giving wrong magnitude of 5th and 7th order.
You can observed it in do_CFFT() function of "C1_N_FFT.c" file as shown below.
// Note :
// As per Dummy data x24.ih_5_load should be 2358.74 and
// x24.ih_7_load should be 1710.125.
if (fft.ph_fftcalc == &fft.r)
{
x24.ih_5_load = mag_buf[5];
x24.ih_7_load = mag_buf[7];
if(x24.ih_5_load < 2300.0)
{
x24.error++;
GpioDataRegs.GPBTOGGLE.bit.GPIO55 = 1;
}
}
Hi Shashank,
I ran your code and the execution does not stop in the error block (for the 5th and 7th bin)
Amtech said:if(x24.ih_5_load < 2300.0) { x24.error++; GpioDataRegs.GPBTOGGLE.bit.GPIO55 = 1; }
Neither do i see an issue in the IFFT, i dont come across the dead spot, here is a snapshot of my CCS
I am running only 1 core. Can you turn off the second core and try to run it again to see if the issue persists.
We have checked code which we shared with you with "c2000 CGT 16.9.6.LTS", and we didn't face any issues.
What is the difference in versions "c2000 CGT 16.9.6.LTS" and "C2000_CGT 6.4.10"?
Is it that this library "c28x_fpu_dsp_library" V1.5 isn't properly supported by older versions like "C2000_CGT 6.4.10", because we didn't find any such note within library's documentation.
Can you check code with version "C2000_CGT 6.4.10"?
Regards,
Shashank.