This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: EnDat-Library PWR CTR needed?

Part Number: TMS320F28379D


Is the PWR CTL GPIO necessary to successfully use the EnDat Library on the C2000 F2837XD.

The IDDK Board is using this pin to enable and disable the Power-Connection to the Encoder.

Since we want to develop a very cheap Hardware for the Encoder-Interface we would like to spare this function to reduce the number of needed ICs.

Will the library still work if we don't use the PWR CTL and just connect the Encoder directly to 5V ?