This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28027F: BOOT TO FLASH Doesn't work

Part Number: TMS320F28027F

Tool/software: Code Composer Studio

Hello! 

I looked for a same problem here, but the tips doesn't work.

I'm using a 28027F microcontroller and i've got a problem with the flash boot, when I reset the microcontroller, the programm stop to work. 

I'm using "F2802x_generic_flash" and I set the S3 to the off position after write the code, the programm run while the microcontroller are not reseted. I changed the linker, but still not working.

Sorry for the bad english...

Regards,

Yuri.