Other Parts Discussed in Thread: TIDM-1001
Hi,
In TIDM-1001, the controller's power is fed by UCC28600EVM. I searched and found that there are two EVM, one is called UCC28600EVM-65W, the other one is called UCC28600EVM. which one is used?
Besides, do I have to make changes to the board because the output of neither evm is 12V.
I'm asking this because we would like to make the board according to the schematics offered in ti.com