Part Number: INSTASPINUNIVERSALGUI
Hello,
I'm having an issue getting past page 12 step 5 in the "GUI Quick Start Guide" due to a connection issue. When I load the application the only connection option that looks remotely similar is "Texas Instruments XDS100v2 USB Debug Probe" and not the one the "GUI Quick Start Guide" Mentions, "Spectrum Digital XDS100v2 emulator". I can't seem to find a resolution to this and without this I can't progress with this user guide or any of teh other provided material.
I'm also seeing an error presumably because of this previously mentioned issue. I have included screen shots below to better explain what I'm seeing. Any help would be VERY helpful.
Kas
I should also add that attempting to run the program under CCS produces an error as well. I have included a image of this below.