This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello, I wanted to ask how to flash using C2prog. I have been trying to flash the code into the ROM using C2prog.
I have used the command specified in the C2prog manual for C2000 but it is giving me error as in
fatal error: cannot open input file "hex2000.out": No such file or directory
gmake[1]: *** [Debug/test.hex ./Debug/test.out] Error 1
gmake[1]: Target 'secondary-outputs' not remade because of errors.
gmake: *** [all] Error 2
What should i do to make it correct. Any help is greatly appreciated.
Thanking in ahead of time,
Regards,
Akhil