This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: need four pwm waves with high resolution

Part Number: TMS320F28035

hello sir/madam,

our product have 2 LLC topology work in parallel.

in order to equal the current through these 2 LLC, we have a solution that need 2 pairs of pwm waves with different frequencies(1 pair for 1 LLC topology with 2 pwm waves phase shifted 180 degree from each other) and the pwm resolution less than 0.05KHz(the work frequency is between 100kHz and 300kHz).

it seems that tms320f28035 cannot have the capability to have 4 HRPWM with different frequencies.

1. please help to confirm my opinion above.

2. do you have any other solution for the 4 high resolution pwm generation?

3.do you have any other solution for current balance for 2 LLC work in parallel?

i am look forward for your relay.

thank you.