This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are using a Delfino F28377D controlCARD (TMDSCNCD28377D) to operate and control a power converter. However, while feeding the power converter with high voltage dc input and after a while (30s to 2min or more), suddenly the DSP sets all outputs to low (or high impedance). This failure must be connected to power supplying issues of the control card, EMI or noise. We have been wondering if there is some control register, led on the card, or pin, that we can monitor in order to determine the state or (even better) the reason the CPU enters this mode of operation.
Any help will be highly appreciated,
Panagis Vovos
Dept. of Electrical and Computer Engineering
University of Patras, Greece