This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: launchPad f28379d

Part Number: LAUNCHXL-F28379D

Dear Support,

I run usb_dev_bulk_cpu01 example on LAUNCHXL-F28379D evaluation board. This board doesn't have USB connector, but I thought that  

uint32_t status = USBModeGet(USB0_BASE); should get correct status( all status values exist in usb.h file)

But I get status 0x98 . What status should I get ?  USB_DUAL_MODE_DEVICE?

 

...

IntMasterEnable();

uint32_t status = USBModeGet(USB0_BASE);

// Main application loop.

while(1) {}

Thanks,Sabina


 

 

 

 

 

 

 

  • Sabina,

    Our USB expert is out of the office until next week. Because of this, I expect a delay in providing an answer until Tuesday. I will see if anyone can help you before he returns.

    In the meantime if you can provide any additional details regarding the setup that may help provide a response (Dec 5th)

    Regards
    Lori