Part Number: TMS320F28377D
Dear all,
I found there is a isr.cmd in projects of the official examples. My question is:
1) what's the isr.cmd for. is it working as a accessory definition of main CMD file? for example, only assign a ram for running interrupt functions
2) My project already has a .TI.ramfunc section for using ram for interrupt functions. In this case, should I just ignore the isr.cmd or just remove the file from project.
.TI.ramfunc section:
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
//.TI.ramfunc : {} > RAMM0, PAGE = 0
.TI.ramfunc : {} > RAMLS0 | RAMLS1 | RAMLS2 | RAMGS13 , PAGE = 0 //---xhf,coordinating with flash
#else
ramfuncs : > RAMM0 PAGE = 0
#endif
#endif
"isr.cmd":
MEMORY
{
PAGE 0 : /* Program Memory */
PAGE 1 : /* Data Memory */
}
/*
Allocate sections to memory blocks.
*/
SECTIONS
{
/* Allocate program areas: */
isrfunc : LOAD = RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4,
RUN = RAMGS14, // good, cpu02 hasing the ramgs14
LOAD_START(_isrfuncLoadStart),
LOAD_END(_isrfuncLoadEnd),
RUN_START(_isrfuncRunStart),
LOAD_SIZE(_isrfuncLoadSize),
PAGE = 0
}