Other Parts Discussed in Thread: MOTORWARE
Hi,
We are bringing up a new project and getting ready to settle on a version of Motorware to start developing our application code on for a production product.
However, I am trying to determine which lab to base our software on and move forward with. I was wondering if there is a recommended solution after the board bring up process has been completed.
Lab11 looks to be the simplest most basic motor control lab. Nothing fancy, no motor ID, no rs online, just FAST with a software FOC. This could work, but I think Rs Online might help us as the motors are pretty small high current motors. I think it would be wise to have it.
Lab11a Adds the 'InstaSpin' features. This looks like it is only Rs Online and the trajectory calculation? With the trajectory basically just being a simple ramp (using the 027F, so no Motion).
Lab20 I am not entirely sure why this exists and could use some clarification, because I feel like there is something I am missing. It looks like this lab should really fall somewhere before Lab 11. Its still using the control object, but it is only using the PI controllers. Are the ROM PI controllers better/more capable than the code based ones provided? Am I missing something else? Lab21 could have been implemented using Lab11+ as a base rather than Lab20, right (not that Lab21 is applicable to me)? Does this include Rs Online or motor ID?
Thanks for the clarification!
Jim