Other Parts Discussed in Thread: SM320F28335-HT
Hello Champs!
We would like to evaluate the feasibility of using the SM320F28335-HT device in one of our upcoming designs. I see that this product is on the roadmap but not yet available in Hi-Rel. Can someone please shed some light on availability. I would like to know availability of the entire development environment not just the device. For example, development boards and and other tools.
Also, I would like to know if any of the products in the Stellaris family available or will be available in Hi-Rel.
Here is info I found about the available products and roadmap.
http://focus.ti.com/hirel/docs/productcontent.tsp?sectionId=605&tabId=2412
High Temperature (HT) Roadmap Products
| Device | Function |
| Data Converters | |
| ADS8320-HT | 16-Bit, High-Speed, microPower Sampling ADC |
| Power | |
| TPS62110-HT | Adjustable, 700-mA, 17-V Vin Step-Down Converter |
| Amplifiers | |
| OPA129-HT | Ultra-Low Bias Current Diff Operational Amplifier |
| INA117-HT | High Common-Mode Voltage Difference Amplifier |
| INA271-HT | Voltage Output High-Side Current Shunt Monitor |
| Reference | |
| Processors | |
| SM320F28335-HT | 32-Bit Floating Point Motor Control DSP |
| OMAP-L137-HT | Low-Power Applications Processor (ARM9 + DSP) |
Thanks,
Krishna Allam
Schlumberger Oilfield Services
Formation Evaluation Integration Center
110 Schlumberger Dr., MD 10
Sugar Land, TX 77478
(281) 285-8432 office