This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100 USB to Serial problem

Hello,

 

We use the XDS100v1 reference design on our board with a controlCARD F28335 Rev1.1(R24 removed)  and the JTAG interface works like a charm with CCS4.1. Not so the USB to serial part. The USB Serial Port is registert in windows and i can connect to it, and i receive data everytime i send it from the dsp. The problem is that the data is not the same that was transmitted by the dsp, the SCI_echoloopback program for example put this to the terminal (CCS4.1 Terminal):

âÛnòF|ânäb lrä’ÜÆāćnà#Oà;Nì’ÜÆb  âÛnòF|ânäb nrä’ÜÆāć
nà#Oà;Nì’ÜÆb  âÛnòF|ânäb brä’ÜÆāćnà#Oà;Nì’ÜÆb  âÛnòF|ânäb 
brä’ÜÆāćnà#Oà;Nì’ÜÆb  âÛnòF|ânäb nrä’ÜÆāćnà#Oà;Nì’ÜÆb 

 

Now maybe i am missing the obvious, cause i'm quite new to this topic, but i cant imagine what could be wrong here. Any ideas on this?

 

Regards,

Stefan Troeger