Hi,
For type 1 and later PWM modules, there's 1 or 2 clock delay when sync:
My questions are:
1) The delay is between PWM1 and PWM2. What about PWM2, PWM3 and PWM4, are there any delay between them?
2) We'd like to sync 3 PWM modules without any delay, how can we do?
Another issue about sequence between shadow load and compare.
In our application, shadow load is used for CMPA, when CTR=Zero. In up-down mode, when CTR decreased to zero, TWO actions will be done: one is shadow load CMPA, the other is compare CTR and CMPA. What's the sequence of these two actions? Who will be the first? Sometimes, we'd like to set the CMPA to zero by shadow load, and CTR=CMPA=Zero, the AQ works immediately, High or Low.
Thanks a lot.
Br, Jordan