Part Number: TMS320F28375D
I am making a project using CLA to compute an FFT. The FFT code works pretty well on C28x, but when I put it in .cla file, the problems begin.
In the debugger if i do NOT manually "Connect target"&"Load symbols" to CLA, the debug simply can't excute the CLA part. (I use Cla1ForceTask1andWait(); from example projects).
If I Do connect and load, i step-by-step go through the CLA code, but it doesn't cause any changes in data! I tried replacing FFT with some basic operations with arrays, like change selected element, but this was of no use either. I could only see the values I loaded to the array in the main C28x code, but no changes could be done.
I did all the memory management in the .cmd file (code below), but I'm not that good in understanding how to write .cmd, so could have left out something crucial. Guess the problem is somewhere in this file, but I can't determine it.
Thanks in advance!
Regards, Konstantin
--define=CLA_C=1 #if CLA_C // CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start #endif //CLA_C MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x000000, length = 0x000002 RAMM0 : origin = 0x000122, length = 0x0002DE RAMD0 : origin = 0x00B000, length = 0x000800 RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAMD1 : origin = 0x00B800, length = 0x000800 RAMLS0_1 : origin = 0x008000, length = 0x001000 RAMGS0_2 : origin = 0x00C000, length = 0x003000 RAMGS9 : origin = 0x015000, length = 0x001000 RAMGS10 : origin = 0x016000, length = 0x001000 RAMGS11 : origin = 0x017000, length = 0x001000 RESET : origin = 0x3FFFC0, length = 0x000002 PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */ CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 RAMLS2_3 : origin 0x009000, length 0x001000 RAMLS4_5 : origin 0x00A000, length 0x001000 RAMGS3_4 : origin = 0x00F000, length = 0x002000 RAMGS5_6 : origin = 0x011000, length = 0x002000 RAMGS7 : origin = 0x013000, length = 0x001000 RAMGS8 : origin = 0x014000, length = 0x001000 RAMGS12 : origin = 0x018000, length = 0x001000 RAMGS13 : origin = 0x019000, length = 0x001000 RAMGS14 : origin = 0x01A000, length = 0x001000 RAMGS15 : origin = 0x01B000, length = 0x001000 } SECTIONS { codestart : > BEGIN, PAGE = 0 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 .TI.ramfunc : {} > RAMM1, PAGE = 0 #else ramfuncs : > RAMM0 PAGE = 0 #endif #endif CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMLS4_5, PAGE = 1 Cla1Prog : > RAMLS4_5, PAGE =1 .text : >> RAMM0 | RAMM1 | RAMD0 | RAMD1 |RAMGS0_2 /*RAMM0 | RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4*/, PAGE = 0 .cinit : > RAMGS0_2, PAGE = 0 .pinit : > RAMGS0_2, PAGE = 0 .switch : > RAMGS0_2, PAGE = 0 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ .stack : > RAMGS3_4, PAGE = 1 .ebss : > RAMGS8, PAGE = 1 .econst : > RAMGS5_6, PAGE = 1 .esysmem : > RAMGS7, PAGE = 1 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 .bss_cla : > RAMLS4_5, PAGE = 1 //specific items IOBuffer : > RAMLS2_3, ALIGN=512, PAGE=1 //2*256 } /* //=========================================================================== // End of file. //=========================================================================== */