This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: Tms320F28075

Part Number: TMS320F28075


Hi,

 My Control card of TMS320F28075 is not detected as USB. Two LED's of FT2232HL is glowing (pin no. 54 and 55).Also I checked voltage at pin no. 60 i.e. PWREN 3.3V and at pin no. 36 i.e. SUSPEND is 0V. Is my FT2232HL is not working or it is working in other mode. Also what to do to detect as USB.

Regards,

Sagar