This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to TMS320F28069MPZT use mcbsp to implement standard UART communication

hello

who can tell me that how to use  TMS320F28069MPZT with mcbsp to implement standard UART  communication?

detail:

I'm working in motor controlling with DRV8312-69M-KIT and TMDSCNCD28069MISO Piccolo F28069 controlCARD;

now,I want to implement  standard UART  communication with mcbsp and DMA in TMS320F28069MPZT  to communicate with another microchip which support standard UART  communication,then I can adjust the parameters of motor controller.

thanks

  • Hanhua,

    It looks like this is possible. C2000 does not have any source code to share for doing this. However, the C6000 and C5000 devices. The McBSP on these devices is very similar and it should be possible to port the software to F2806x.

    Please take a look at the following Application Reports for reference.
    www.ti.com/.../spra633
    www.ti.com/.../spra661

    I would be curious to see if you are able to port this in the end. Please update us after you complete this!

    Thanks,
    Mark