This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: Power Supply Operating Range

Part Number: TMS320F28375D

Dear TI,


We are using TMS320F28375D DSP in our design. As per datasheet device operating voltage range VDDIO of DSP is 3.14V to 3.47.

What could be the behavior of DSP, if this voltage VDDIO reduced to 3.0V?

With Regards,

Dushyant Rana

  • Dushyant,

    Device performance is not guaranteed below recommended operating voltage range. Also, if the VDDIO goes lower than 3v it will generate a Device reset, since there is a BOR circuit inside the DSP acting as a Voltage supervisor.

    Regards,

    Nirav