Part Number: DRV8312-69M-KIT
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
Dear motorware team,
I am currently trying to compare the electrical position of the FAST estimator to the electrical position incremental encoder in Lab 20. I am using the QEP driver and the enc.c/enc.h module to read out the information of the encoder. The encoder is connected to J4. The code is running fine for about 10 seconds. After that the motor stops spinning and code composer freezes. If I disconnect the encoder then the algorithm with the same code does not freeze.
This also seems to happen to all the other labs as well. When I connect the encoder to J4 running Lab05a for example, the same thing happens: code runs fine for 10 seconds and then it freezes, even though it does not read out any encoder information. Have you ever encountered this issue?
The encoder I am using is the HEDM-5500 B12 (1000 CPR). Datasheet: http://www.mouser.com/ds/2/678/V02-1046EN_DS_HEDM-55xx_2014-11-20-909010.pdf
Kind regards,
Dat