This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: F28069 Control Card Won't Run/Debug...New Issue

Part Number: TMS320F28069M

I have a project in which I'm using the F28069M Control Card.  One of them works just fine, but I can't get CCS to connect to the rest of them.  I suspect it's because CCS is getting confused, because all five cards have connected OK in the past.  I had a similar problem recently because I was mixing up the F28068M with the F28069 cards, but that's not the case this time.

In Control Panel there are two XDS 100 Class Auxiliary Port entries and two XDS 100 Class Debug Port entries.  There is also an entry for a USB Composite Device under USB controllers.  I can uninstall them all, and when I plug the card back in the PC recognizes it and installs new drivers.  However, when I attempt to debug in CCS it gives me this error:

Error connecting to the target:
(Error -1135 @ 0x0)
The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 7.0.48.0)

Power-off, closing CCS, and rebooting the PC in various combinations hasn't helped.  I tried moving the card around to different USB ports.  I also tried deleting the launch configuration in the .launch folder, but still no luck.  I double-checked the boot/debug switches, and they're correct for connecting the debugger.

Is there something else I can do to try and get CCS to recognize the other cards?

Thanks,

Matt