Part Number: TMS320F280049
Team,
-Can you please confirm if the S&H ADC can be started at different time (ie asynchronously)?
The datasheet shows in "Table 5-48 ADC characteristics" for "ENOB: VREFHI = 2.5 V, fin = 100 kHz, SYSCLK from X1, asynchronous ADCs" that it is not supported:
Q: Does it means that asynchronous is not supported at all or that we do not specify or test it? Can asynchronous mode be at all used and under what condition?
-The sampling capacitor seems to be much higher than for the previous devices:
Q: What are the benefit and drawback of having such an high Sampling capacitor value?
Thanks in advance,
Anthony