This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

reload timer0 in f28335

Hi members, I have a problem when I reload a timer0 into the current interrupt service.

I need make a calculus and reload the timer, but the timer is not reload at this time, is another (greather). I make any wrong pass?

Below put the program, in red the part of interest:

 

// TI File $Revision: /main/2 $
// Checkin $Date: July 30, 2009   18:45:40 $
//###########################################################################
//
// FILE:    Example_2833xLedBlink.c
//
// TITLE:   DSP2833x eZdsp LED Blink Getting Started Program.
//
// ASSUMPTIONS:
//
//    This program requires the DSP2833x header files.
//
//
//    As supplied, this project is configured for "boot to SARAM"
//    operation.  The 2833x Boot Mode table is shown below.
//    For information on configuring the boot mode of an eZdsp,
//    please refer to the documentation included with the eZdsp,
//
//       $Boot_Table:
//
//         GPIO87   GPIO86     GPIO85   GPIO84
//          XA15     XA14       XA13     XA12
//           PU       PU         PU       PU
//        ==========================================
//            1        1          1        1    Jump to Flash
//            1        1          1        0    SCI-A boot
//            1        1          0        1    SPI-A boot
//            1        1          0        0    I2C-A boot
//            1        0          1        1    eCAN-A boot
//            1        0          1        0    McBSP-A boot
//            1        0          0        1    Jump to XINTF x16
//            1        0          0        0    Jump to XINTF x32
//            0        1          1        1    Jump to OTP
//            0        1          1        0    Parallel GPIO I/O boot
//            0        1          0        1    Parallel XINTF boot
//            0        1          0        0    Jump to SARAM     <- "boot to SARAM"
//            0        0          1        1    Branch to check boot mode
//            0        0          1        0    Boot to flash, bypass ADC cal
//            0        0          0        1    Boot to SARAM, bypass ADC cal
//            0        0          0        0    Boot to SCI-A, bypass ADC cal
//                                              Boot_Table_End$
//
// DESCRIPTION:
//
//    This example configures CPU Timer0 for a 500 msec period, and toggles the GPIO32
//    LED on the 2833x eZdsp once per interrupt. For testing purposes, this example
//    also increments a counter each time the timer asserts an interrupt.
//
//       Watch Variables:
//          CpuTimer0.InterruptCount
//
//       Monitor the GPIO32 LED blink on (for 500 msec) and off (for 500 msec) on the 2833x eZdsp.
//
//###########################################################################
// $TI Release: DSP2833x/DSP2823x C/C++ Header Files V1.31 $
// $Release Date: August 4, 2009 $
//###########################################################################


#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

// Prototype statements for functions found within this file.
interrupt void cpu_timer0_isr(void);

int control=0; //CODIGO GUILLERMO
int contador=0;

//variables añadidas para la v4
float T=15;  //T es el periodo que deseamos mantener constante
    //el T no hay que ponerlo en 15e-6, ya que los tiempos que calcularemos
    //estan en esa base
float num=0,den=0;
float calculo_resto_ton=0;
//fin variables añadidas v4
 
float tiempo=5;
 
 
 
void main(void)
{

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();  // Skipped for this example


// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
   EALLOW;  // This is needed to write to EALLOW protected registers
   PieVectTable.TINT0 = &cpu_timer0_isr;
   EDIS;    // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize the Device Peripheral. This function can be
//         found in DSP2833x_CpuTimers.c
   InitCpuTimers();   // For this example, only initialize the Cpu Timers
#if (CPU_FRQ_150MHZ)
// Configure CPU-Timer 0 to interrupt every 500 milliseconds:
// 150MHz CPU Freq, 50 millisecond Period (in uSeconds)
   ConfigCpuTimer(&CpuTimer0, 150, 2.6);
#endif
#if (CPU_FRQ_100MHZ)
// Configure CPU-Timer 0 to interrupt every 500 milliseconds:
// 100MHz CPU Freq, 50 millisecond Period (in uSeconds)
   ConfigCpuTimer(&CpuTimer0, 100, 500000);
#endif

// To ensure precise timing, use write-only instructions to write to the entire register. Therefore, if any
// of the configuration bits are changed in ConfigCpuTimer and InitCpuTimers (in DSP2833x_CpuTimers.h), the
// below settings must also be updated.

   CpuTimer0Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0

// Step 5. User specific code, enable interrupts:

// Configure GPIO32 as a GPIO output pin
   EALLOW;
   //en el programa original es el puerto 32 que corresponde al led
   GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
   GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
   GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0;
   GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;
   EDIS;

// Enable CPU INT1 which is connected to CPU-Timer 0:
   IER |= M_INT1;

// Enable TINT0 in the PIE: Group 1 interrupt 7
   PieCtrlRegs.PIEIER1.bit.INTx7 = 1;

// Enable global Interrupts and higher priority real-time debug events:
   EINT;   // Enable Global interrupt INTM
   ERTM;   // Enable Global realtime interrupt DBGM

// Step 6. IDLE loop. Just sit and loop forever (optional):
   for(;;)
   {
   }
}


interrupt void cpu_timer0_isr(void)
{
 GpioDataRegs.GPASET.bit.GPIO2 = 1; // on GPIO2


 num=2475-2000;
 den=2100-2000;
 calculo_resto_ton=num/den;
  
 ConfigCpuTimer(&CpuTimer0, 150,calculo_resto_ton );

 // Acknowledge this interrupt to receive more interrupts from group 1
 PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
 CpuTimer0Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0

GpioDataRegs.GPACLEAR.bit.GPIO2 = 1;  //Set GPIO down

}

//===========================================================================
// No more.
//===========================================================================