Part Number: TMS320F28069
Tool/software: Code Composer Studio
Hi,
I'm currently using the F28069 for digital power control.
My project and controls are working.
I just noticed that the boot up time for my processor seems to be around 100mS.
Meaning from the time VDD reaches 3.3V to when I start outputting PWMs.
I do have code/conditions which will add a little delay until I output PWMs but I don't think it would add up to longer than a 1ms.
So my question is, what is the normal boot up time for the F28069 ?
Timer from getting 3.3V to starting to execute code ?
Are there registers I can configure to speed up the boot up process ?
Does 100mS seem normal ?
thanks!