This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Very low speed. Error 1007

Part Number: LAUNCHXL-F28069M

Hello,

I run lab13e to control motor at very low speed. It works at speed 0.01RPM. But this speed I can reach only when motor previously running on higher speed(e.g. 1rpm). When motor is stopped I cannot set so low speed. I get error 1007. The minimum speed what can I set when motor stopped is only 0.06RPM ( with parameters USER_NUM_ISR_TICKS_PER_CTRL_TICK and USER_NUM_CTRL_TICKS_PER_SPEED_TICK).

I would like to ask why I cannot set directly so low speed or which parameters I have to focus, if there any?