Hi, Champs,
As I stated in below post: https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/648540
My customer is now using F280049M at room temperature without trim, however, out of 3 parts there're 2pcs running the clock outside the spec of +/-3% accuracy.
It's confirmed that the Vdd is 1.177v, within range of 1.14~1.32v, but the clock is about 9.2MHz by measuring XCLKOUT on these 2 devices, no matter it's INTOSC1 or INTOSC2.
Please check attached waveforms and advise what needs to be checked, or if those samples are not validated for the accuracy item?
Best Regards,
Ricky Zhang