Part Number: TMS320F28069M
Other Parts Discussed in Thread: DRV8305, MOTORWARE,
Hi,
I am using the TMS320F28069M and a DRV8305 motor driver, and we have the Motorware libraries installed. I dug through the DRV8305 datasheet hoping that there was a simple way to implement current limiting to the motor. The options relating to current limiting seemed to be 1: shut off and send a warning. 2: dont shut off but send a warning. 3: dont shut off or send a warning. Due to the nature of the project, a hard shut-off is not acceptable and we are looking to limit the current to the motor, but allow it to continue running at max current indefinitely. Our main ISR on the TSM is running at 100Hz which is slower than we would want for a current limiting loop but changing that frequency is out of the question. What options exist for implementing current limiting as described in this application using the motorware libraries? Which of the Labs would you suggest I look at?