Part Number: TMS320F280049
Looking to save a pin in a tight HW design...
The goal is to route eQEP-1 Strobe (configured as an output) internally to EXTSYNCIN2 (through input X-Bar). This should be achievable with the Input XBAR: Input X-BAR INPUT6 has a connection to EXTSYNCIN2 (per Figure 7-1 of TRM). I assume there is no issue with using the input side of QEP1 strobe output at a pin to feed the XBAR (no special case here). If there is any reason for concern, please let me know.
Regards,
Eric