This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: Pin mapping of TMS320F28035 on the docking stn

Part Number: TMS320F28035
Other Parts Discussed in Thread: C2000WARE

I have a question regarding the pin configuration of piccolo TMS320F28035. I am using Ti Docking stn USB -EMU R[3] with it.

I want to access Pin 73(GPIO 1) and Pin 74 (GPIO 2) of piccolo TMS320F28035. on the docking station. I cant find pin 73,74 on docking station. Can anyone help with it? Thank you!

  • Hi Sagar,

    GPIO 1 is pin 01 on J4 of your board and GPIO 2 is pin 02 on J5 of your board.

    Do you have C2000Ware installed? If not, I would suggest installing it. It has the schematics for your boards and a lot of good programming examples to use.

    Once you have it installed, go to the following directory and open "USBDockingStation_Schematic_[R3]" for the schematic:

    C:\ti\c2000\C2000Ware_1_00_02_00\boards\ExperimenterKits\DockingStation_DIM_100pin\R3

    This should help you with finding what pins on your docking station link up to your controlCard.

    Hope this helps,
    Kevin