This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: Pick&Place Files for F28069 Piccolo controlCards

Part Number: TMS320F28069


Hello,

My customer is looking into building both the F28069 Piccolo controlCARD as well the Piccolo TMS320F28069 Isolated controlCARD . For that the need a Pick-and-Place description document that consists on a series of (x,y) coordinates for the placement machine. We are aware that there are Gerber files and Schematics, among other things, in the Control Suite. But that´s not enough to directly build.

Do we have a Pick&Place document for this board, so they can accelerate the manufacturing process of the boards?

Thanks,
Simon

[unlock] 3/12/18>[LE]

  • Simon,

    I have the pick-and-place files for the F28069ISO, but not for the F28069 cCARD. I have attached the ISO file here, it should be correct.

    Note: ControlCARDs are not intended to be used in a end application, they're for evaluation only. Customers are required to design, build and test their own boards.

    Assembly Report for {TEX116}F2806xISOcontrolCARDr0.4.pcb on 1/14/2014 6:00:43 PM
    
    Name    Part Type       Pins SMD  Position X   Position Y   Rotation  Layer Name      
    -------------------------------------------------------------------------------------
    C1      100-00106       2    Yes  2635.000     1120.000     180.0     Secondary Side  
    C2      100-00125       2    Yes  1525.000     1000.000     270.0     Secondary Side  
    C3      100-00125       2    Yes  1630.000     880.000      180.0     Secondary Side  
    C4      100-00125       2    Yes  1725.000     1000.000     90.0      Secondary Side  
    C5      100-00125       2    Yes  1620.000     1115.000     0.0       Secondary Side  
    C6      100-00125       2    Yes  1730.000     760.000      90.0      Secondary Side  
    C7      100-00125       2    Yes  1535.000     760.000      90.0      Secondary Side  
    C8      100-00125       2    Yes  1595.000     610.000      90.0      Secondary Side  
    C9      100-00125       2    Yes  1670.000     610.000      90.0      Secondary Side  
    C10     100-00003       2    Yes  1640.000     880.000      180.0     Primary Side    
    C11     100-00118       2    Yes  2455.000     1120.000     0.0       Secondary Side  
    C12     100-00118       2    Yes  2140.000     1130.000     180.0     Secondary Side  
    C13     100-00118       2    Yes  1900.000     765.000      270.0     Secondary Side  
    C14     100-00118       2    Yes  2225.000     305.000      0.0       Secondary Side  
    C15     100-00118       2    Yes  2725.000     640.000      0.0       Secondary Side  
    C16     100-00118       2    Yes  2690.000     825.000      180.0     Primary Side    
    C17     100-00118       2    Yes  1845.000     535.000      270.0     Secondary Side  
    C18     100-00118       2    Yes  1860.000     1010.000     180.0     Primary Side    
    C19     100-00118       2    Yes  2585.000     1035.000     0.0       Primary Side    
    C20     100-00118       2    Yes  2155.000     1035.000     0.0       Secondary Side  
    C21     100-00118       2    Yes  1795.000     700.000      270.0     Primary Side    
    C22     100-00118       2    Yes  2380.000     295.000      180.0     Secondary Side  
    C23     100-00118       2    Yes  2540.000     555.000      270.0     Secondary Side  
    C24     100-00118       2    Yes  2545.000     860.000      90.0      Secondary Side  
    C25     100-00122       2    Yes  3310.000     225.000      180.0     Primary Side    
    C26     100-00003       2    Yes  3340.000     365.000      270.0     Secondary Side  
    C27     100-00006       2    Yes  3185.000     350.000      270.0     Primary Side    
    C28     300-00011       2    Yes  3250.000     360.000      270.0     Secondary Side  
    C29     100-00003       2    Yes  3335.000     485.000      180.0     Secondary Side  
    C30     100-00107       2    Yes  1970.000     275.000      90.0      Primary Side    
    C31     100-00107       2    Yes  2310.000     290.000      270.0     Primary Side    
    C32     300-00011       2    Yes  820.000      1010.000     270.0     Secondary Side  
    C33     100-00003       2    Yes  735.000      1010.000     90.0      Secondary Side  
    C34     100-00006       2    Yes  835.000      875.000      270.0     Primary Side    
    C35     300-00012       2    Yes  655.000      1010.000     90.0      Secondary Side  
    C46     SM/C_0402       2    Yes  350.000      500.000      0.0       Secondary Side  
    C47     SM/C_0402       2    Yes  350.000      545.000      0.0       Secondary Side  
    C55     SM/C_0402       2    Yes  310.000      660.000      90.0      Secondary Side  
    C56     SM/C_0402       2    Yes  315.000      295.000      90.0      Secondary Side  
    C57     SM/C_0402       2    Yes  555.000      260.000      0.0       Secondary Side  
    C58     SM/C_0402       2    Yes  630.000      620.000      180.0     Secondary Side  
    C59     SM/C_0402       2    Yes  170.000      495.000      270.0     Secondary Side  
    C60     SM/C_0402       2    Yes  230.000      320.000      90.0      Secondary Side  
    C61     SM/C_0402       2    Yes  645.000      930.000      0.0       Primary Side    
    C62     SM/C_0402       2    Yes  790.000      730.000      90.0      Primary Side    
    C63     SM/C_0402       2    Yes  430.000      215.000      180.0     Secondary Side  
    C64     SM/C_0402       2    Yes  590.000      400.000      270.0     Secondary Side  
    C65     SM/C_0402       2    Yes  490.000      545.000      180.0     Secondary Side  
    C66     SM/C_0402       2    Yes  490.000      500.000      180.0     Secondary Side  
    C67     SM/C_0402       2    Yes  1020.000     1075.000     180.0     Secondary Side  
    C68     SM/C_0402       2    Yes  1255.000     1075.000     0.0       Secondary Side  
    C69     SM/C_0402       2    Yes  1040.000     595.000      180.0     Secondary Side  
    C70     SM/C_0402       2    Yes  1305.000     645.000      90.0      Secondary Side  
    C71     300-00083       2    Yes  1130.000     1145.000     180.0     Secondary Side  
    C200    100-00122       2    Yes  3110.000     905.000      0.0       Primary Side    
    C201    SM/C_0805       2    Yes  3405.000     1060.000     90.0      Secondary Side  
    C202    100-00122       2    Yes  3110.000     800.000      0.0       Primary Side    
    D2      C0805_LED       2    Yes  885.000      230.000      180.0     Primary Side    
    D3      C0805_LED       2    Yes  885.000      330.000      180.0     Primary Side    
    D200    MBRM110ET1GOSCT 2    Yes  2995.000     860.000      180.0     Secondary Side  
    FID1    FID40           1    Yes  65.000       1135.000     0.0       Primary Side    
    FID2    FID40           1    Yes  3485.000     1135.000     0.0       Primary Side    
    FID3    FID40           1    Yes  3485.000     205.000      0.0       Primary Side    
    FID4    FID40           1    Yes  65.000       1135.000     0.0       Secondary Side  
    FID5    FID40           1    Yes  3485.000     1135.000     0.0       Secondary Side  
    FID6    FID40           1    Yes  3485.000     205.000      0.0       Secondary Side  
    J1      320-00004       11   No   325.000      860.000      180.0     Primary Side    
    J200    A97799CT-ND     9    Yes  3245.000     1105.000     180.0     Primary Side    
    L1      130-00042       2    Yes  2460.000     1040.000     0.0       Secondary Side  
    L2      130-00042       2    Yes  2295.000     1130.000     0.0       Secondary Side  
    L3      130-00042       2    Yes  1810.000     770.000      270.0     Secondary Side  
    L4      130-00042       2    Yes  2080.000     305.000      180.0     Secondary Side  
    L5      130-00042       2    Yes  2655.000     530.000      90.0      Secondary Side  
    L6      130-00042       2    Yes  2645.000     870.000      270.0     Secondary Side  
    L7      130-00042       2    Yes  1770.000     530.000      90.0      Secondary Side  
    L8      130-00043       2    Yes  1855.000     1030.000     180.0     Secondary Side  
    L21     0805            2    Yes  470.000      405.000      270.0     Secondary Side  
    L22     0805            2    Yes  370.000      405.000      270.0     Secondary Side  
    LD1     200-00001       2    Yes  3315.000     650.000      180.0     Primary Side    
    LD2     200-00002       2    Yes  3315.000     735.000      180.0     Primary Side    
    LD3     200-00002       2    Yes  3315.000     820.000      180.0     Primary Side    
    LD4     200-00001       2    Yes  730.000      1125.000     180.0     Primary Side    
    M1      VIA_TP_13_30    1    No   1305.000     1075.000     0.0       Primary Side    
    M2      VIA_TP_13_30    1    No   1305.000     1025.000     0.0       Primary Side    
    M3      VIA_TP_13_30    1    No   1305.000     975.000      0.0       Primary Side    
    M4      VIA_TP_13_30    1    No   1295.000     785.000      0.0       Primary Side    
    M5      VIA_TP_13_30    1    No   1295.000     735.000      0.0       Primary Side    
    M6      VIA_TP_13_30    1    No   1300.000     305.000      0.0       Primary Side    
    M7      VIA_TP_13_30    1    No   1310.000     545.000      0.0       Primary Side    
    M8      VIA_TP_13_30    1    No   1300.000     255.000      0.0       Primary Side    
    M200    VIA_TP_13_30    1    No   2895.000     995.000      0.0       Primary Side    
    M201    VIA_TP_13_30    1    No   3365.000     890.000      0.0       Primary Side    
    M202    VIA_TP_13_30    1    No   2895.000     1050.000     0.0       Primary Side    
    M203    VIA_TP_13_30    1    No   2895.000     1105.000     0.0       Primary Side    
    M204    VIA_TP_13_30    1    No   3320.000     890.000      0.0       Primary Side    
    M205    VIA_TP_13_30    1    No   3275.000     935.000      0.0       Primary Side    
    M206    VIA_TP_13_30    1    No   3275.000     890.000      0.0       Primary Side    
    M207    VIA_TP_13_30    1    No   3405.000     890.000      0.0       Primary Side    
    P1      120-00066       100  Yes  350.000      53.150       0.0       Primary Side    
    Q200    402-00039       3    Yes  3170.000     1050.000     0.0       Secondary Side  
    R1      110-00234       2    Yes  2300.000     1030.000     0.0       Secondary Side  
    R2      110-00235       2    Yes  2540.000     720.000      90.0      Secondary Side  
    R3      110-00172       2    Yes  1900.000     270.000      90.0      Primary Side    
    R4      310-00011       2    Yes  3320.000     650.000      180.0     Secondary Side  
    R5      110-00085       2    Yes  3320.000     735.000      180.0     Secondary Side  
    R6      110-00085       2    Yes  3320.000     820.000      180.0     Secondary Side  
    R7      110-00235       2    Yes  1970.000     1130.000     180.0     Secondary Side  
    R8      310-00034       2    Yes  780.000      1125.000     270.0     Secondary Side  
    R9      110-00236       2    Yes  3040.000     455.000      270.0     Secondary Side  
    R10     110-00236       2    Yes  3110.000     455.000      270.0     Secondary Side  
    R11     110-00237       2    Yes  3045.000     615.000      90.0      Secondary Side  
    R12     110-00237       2    Yes  3110.000     615.000      90.0      Secondary Side  
    R24     0402            2    Yes  245.000      665.000      180.0     Secondary Side  
    R72     SM/R_0402       2    Yes  455.000      750.000      270.0     Primary Side    
    R73     SM/R_0402       2    Yes  270.000      220.000      0.0       Secondary Side  
    R74     SM/R_0402       2    Yes  590.000      520.000      90.0      Secondary Side  
    R75     SM/R_0402       2    Yes  700.000      595.000      90.0      Secondary Side  
    R76     SM/R_0402       2    Yes  700.000      505.000      270.0     Secondary Side  
    R77     SM/R_0402       2    Yes  240.000      780.000      180.0     Primary Side    
    R78     SM/R_0402       2    Yes  745.000      445.000      90.0      Secondary Side  
    R79     SM/R_0402       2    Yes  725.000      375.000      180.0     Secondary Side  
    R81     SM/R_0402       2    Yes  740.000      230.000      0.0       Primary Side    
    R82     SM/R_0402       2    Yes  740.000      330.000      0.0       Primary Side    
    R84     SM/R_0402       2    Yes  165.000      300.000      270.0     Secondary Side  
    R200    SM/R_0402       2    Yes  2955.000     1050.000     0.0       Primary Side    
    R201    SM/R_0402       2    Yes  2955.000     1105.000     0.0       Primary Side    
    R202    SM/R_0402       2    Yes  3315.000     1025.000     90.0      Secondary Side  
    R203    SM/R_0402       2    Yes  3265.000     1025.000     90.0      Secondary Side  
    R204    SM/R_0402       2    Yes  3235.000     910.000      90.0      Primary Side    
    R205    SM/R_0402       2    Yes  3345.000     940.000      0.0       Primary Side    
    R206    SM/R_0402       2    Yes  2945.000     1070.000     270.0     Secondary Side  
    R207    SM/R_0402       2    Yes  3115.000     970.000      0.0       Secondary Side  
    R208    SM/R_0402       2    Yes  3075.000     1140.000     180.0     Secondary Side  
    RN1     310-00017       16   Yes  1440.000     1070.000     180.0     Primary Side    
    RN2     310-00017       16   Yes  1440.000     870.000      180.0     Primary Side    
    RN3     310-00018       16   Yes  2690.000     635.000      0.0       Primary Side    
    SW1     206-00010       4    Yes  3085.000     575.000      0.0       Primary Side    
    SW2     206-00009       6    Yes  1665.000     470.000      270.0     Primary Side    
    SW3     206-00010       4    Yes  1425.000     470.000      0.0       Primary Side    
    TP1     280-00010       1    No   3110.000     265.000      0.0       Primary Side    
    TP2     280-00010       1    No   3110.000     355.000      0.0       Primary Side    
    TP3     280-00010       1    No   3185.000     440.000      0.0       Primary Side    
    TP4     280-00010       1    No   595.000      1125.000     270.0     Primary Side    
    TP5     280-00010       1    No   865.000      1125.000     270.0     Primary Side    
    U1      TMS320F28069U-P 101  Yes  2230.000     725.000      180.0     Primary Side    
    U2      202-00157       6    Yes  1625.000     1000.000     180.0     Secondary Side  
    U3      202-00157       6    Yes  1630.000     755.000      0.0       Secondary Side  
    U4      296-24289-1     9    No   3295.000     370.000      0.0       Primary Side    
    U5      202-00154       6    Yes  3275.000     535.000      90.0      Primary Side    
    U6      203-00043       5    Yes  780.000      1010.000     270.0     Primary Side    
    U15     768-1024-2-ND   64   Yes  380.000      430.000      270.0     Primary Side    
    U16     93LC56C-I/SN-ND 8    Yes  820.000      495.000      0.0       Primary Side    
    U18     296-21883-1-ND  5    Yes  360.000      750.000      0.0       Primary Side    
    U19     SOIC-8          8    Yes  1130.000     1000.000     0.0       Primary Side    
    U20     SOIC-8          8    Yes  1130.000     760.000      0.0       Primary Side    
    U21     SOIC-8          8    Yes  1130.000     520.000      0.0       Primary Side    
    U22     SOIC-8          8    Yes  1130.000     280.000      180.0     Primary Side    
    U200    296-21265-1-ND  5    Yes  3045.000     1055.000     90.0      Secondary Side  
    X1      405-00009       4    Yes  2150.000     280.000      0.0       Primary Side    
    Y2      XC1118CT-ND     4    Yes  670.000      775.000      90.0      Primary Side    
    -------------------------------------------------------------------------------------
    
    Rename to *.xyr

    Regards,
    Cody 

  • Thanks Cody,

    This resolved our issue, at least for the ISOcard.

  • Saimon,

             do you need the non-ISO F28069 files? I may be able to get them for you, This will not be a trivial effort so please only request the if you actually need them.

    If you require them you should expect to wait several weeks.

    Regards,
    Cody 

  • Simon,

    the non-ISO F28069 controlCARD pick and place file can be found in the attachment.

    F28069ControlCardr1.1.txt (rename to *.xyr)


    Regards,
    Cody