Part Number: TMS320C28341
Other Parts Discussed in Thread: TMS320F2808,
Hello,
I am designing lightning protection circuitry around the I/O pins for the TMS320F2808 processor. I couldn’t find this in the input menu, so I chose one close. The test waveforms to be injected on the input connector pins conform to the airborne standard RTCA/DO160G Section 22, waveforms 3/3 and 4/1 at level 3.
My approach is to augment the internal clamp diodes with external schottky clamps, as illustrated below:
My question is; what is the nominal forward drop across the internal clamp diodes for the GPIO I/O pins for this processor?
I have simulated this with a relatively high drop schottky, the MBR21011CT, but I am just guessing.
Also, I assume that the maximum spec for input clamp current (±20ma) refers to the maximum current through the internal clamp diodes.
Thanks,
Larry Richardson