I took the hardware used in the solar EMU and designed hardware for 250W. The hardware uses a Piccolo LaunchPad. I have loaded the code from the Solar Explorer Kit into the LaunchPad. I checked the PWM signals the the power stage and they are what I expect. My question is how can I continue to test the code in the LaunchPad to verify the signals are on the correct pins:
1. When I added the LaunchPad to the hardware one of my drivers on my hardware shorted and failed. I did some test of the hardware before adding the LaunchPad to my hardware. I was planning to us the 3.3V and 5V from my hardware to power the LaunchPad. This may not be the best approach.
2. Is it possible to change the duty cycle for the code in the LaunchPad using an external source?
3. Is it possible to run the code open loop at a fixed duty?
Thanks for the help,
Roger