Part Number: TMS320F28377D
Other Parts Discussed in Thread: IEC60730SWPACKAGES
Hello,
We downloaded IEC60730SWPACKAGES and trying f2837xd_test_application with TMS320F28377D.
My customer wants to enable/disable the jump to NMI at Flash_performECCCalculation().
The call is found in Ln-228 of [stl_flash.c].
We once expected the ECC_ENABLE.ENABLE field, but it didn't work. Whichever the field was 0xA or not, NMI was called -- STL_Flash_uncorrectableErrorNMIISR() .
Then, can I ask a question, are there any ways to enable/disable calls to NMI when Flash_performECCCalculation(), or FECC_CTRL.DO_ECC_CALC are used ?
Duplication:
- import the f2837xd_test_application to CCS.
- put the attached file int othe project.
- build and debug run.
- write the variable IsEccEnable with 1 or zero.
/cfs-file/__key/communityserver-discussions-components-files/171/stl_5F00_flash_5F00_Edit.c